Markenheldfoto

Bayline, Armação de Pêra, Vanguard Properties & AEG

Anchored in the south of Portugal, the Algarve is well known for its beautiful coastline and friendly people. 
Designed by architects Saraiva + Associados
Bayline is expected to be completed by the end of the first quarter, 2023.

Blessed with beautiful sandy beaches, picturesque villages and a fabulous climate, it is not surprising that this region is considered the most important tourist region in Portugal. It is also the perfect place to invest.

Located in the unrivalled surroundings of Lagoa dos Salgados and Praia Grande Bay, Bayline is the only resort in Algarve facing the ocean. 

– 256 apartments
– Beachfront location
– 2 hectares of private gardens
– Outdoor pools
- Spa & gymnasium

With 256 apartments in buildings of up to six floors, the luxury private condominium has 2 hectares of private gardens, indoor and outdoor pools, spa, gymnasium, and a games court. And, of course, it has direct access to the beach. The project, under the responsibility of Saraiva + Associados design team, presents a contemporary architecture developed with excellent finishings, terraces and large exterior spans to maximize the luxuriousness of the views. The kitchens are naturally equipped with AEG to match this highly, prestigious development.

Appliances installed:
Brand: AEG 
– Ovens
– Induction hobs
– Extractor hoods
– Built-in microwaves
– Wine coolers
– Built-in washer-dryers
– Built-in refrigerators
– Built-in dishwashers

Schwestermarken