COLMEF

COLMEF Srl has been operating since 1980 in the building sector, developing three main brands: COLMEF, PIETRE D’ARREDO and GEODRY.

PIETRE D'ARREDO is the brand dedicated to the production of reconstructed stones. It was born in Umbria, in the green heart of Italy. Here, history, the culture of stone and with it the tradition of building, are the very core of the identity of the craftsmen of the past, who skillfully sculpting and moulding the stone, created our medieval towns of such enchanting and eternal beauty. Preserving this expertise and the passion for stone, we have invested in research and technology to offer a unique and prestigious product, recreating with our own hands the masonry that has given life to these spectacular surroundings and that will do the same for yours. COLMEF implements autonomously all stages of the production chain, from the selection of the stone for the realization of dies and moulds, up to the production of the stone itself, of the adhesives, of the grouts and of all the products required for the treatment.

GEODRY is the specialised division of COLMEF dedicated to the development of construction systems for waterproofing. GEODRY was born from the experience of COLMEF in the field of technical materials for construction and integrated research in the field of plastic materials with the qualities of adhesives and sealants. GEODRY systems solve the main issues which occur during the installation stage and provide the designers with operating flexibility and customised solutions. The technology of the materials, paired with a simple and fast installation, lowers the human error risk, costs and implementation times, the interference from atmospheric agents.
GEODRY solutions guarantee functionality, durability, ease of maintenance and provide new construction opportunities on any type of substrates, both old and new.


Brand logo
119 followers

Contact

+39 075 923561Sede Legale: Zona Ind. Ponte d’Assi - 06024 Gubbio (PERUGIA)Sede Amministrativa, Via Topino, 11 Zona Ind. Padule06024 Gubbio (PERUGIA)ITALY