Natural flooring
Product news

Natural flooring

At Forbo Flooring Systems, we have been inspired by what is all around us and we are convinced that our best engineer is nature. With its help, we have created Marmoleum.

Marmoleum is a unique linoleum floor covering made of natural raw materials such as linseed oil, wood flour, limestone, resin and jute. These raw materials are obtained from their natural habitat.

Linseed oil is pressed from the seeds of the flax plant. The linseed oil is heated together with pine resin to form a linoleum paste. To this paste we add wood flour, a waste product from the certified forestry industry. Limestone is available in abundance and is the fourth ingredient added to the linoleum mixture to make linoleum granules. Organic pigments and natural iron oxide provide the colouring for the granules. The fibres of the jute plant are used for the jute mesh carrier on which linoleum is calandered.

CO2 neutral from cradle to gate. Marmoleum is a sustainable floor that is CO2 neutral from its origin to the final product, without offsetting.

The raw materials used for creating Marmoleum are rapidly renewable and have absorbed such an amount of CO2 during the time the plants, trees and crops have grown, that this amount of CO2 exceeds the amount of CO2 that is emitted during the production process. Our Marmoleum is produced in a modern, energy efficient environment. We produce with 100% green electricity derived from the sun and wind, not adding any CO2.

By learning to work with our planet and its organic cycles, we are able to make one of the most sustainable floor coverings. Marmoleum has been awarded a large array of international environmental certificates such as the Nordic Swan and the Blue Angel. In addition Marmoleum floor covering improves the environmental and well-being score in building rating schemes such as LEED, Breeam and the Well building standard.