HAHN Lamellenfenster GmbH – The company profile of the louvre window inventor
The roots of the Frankfurt-based company GLASBAU HAHN go back to the year 1829, founding year of the joinery and glazing company J. R. Schön. In 1870, under the direction of Heinrich Hahn, the Company became known as Glaserei & Glashandel HAHN.
HAHN has been involved with natural ventilation since the 1950s.
Since then, the "HAHN Louvres" have set a standard in the field of ventilation, and are synonymous with innovation and quality. Louvre windows are customized: with a wide range of single, double or triple glazing or insulated panels, with wooden or aluminium blades or even with special materials such as stone panels. They protect against ball strikes, are burglar-resistant, fall protection safe, sound insulation certified and can be used for smoke extraction as well as for daily ventilation. HAHN louvre windows can either semlessly integrated into a facade or stand out as an attractive part of its design.
Architects and construction companies use HAHN louvre windows to benefit from the experience of an industry expert that has made its name in the field of individual solutions.
Sus datos personales pueden compartirse con fabricantes externos en función de su actividad en la plataforma. Puede optar por no participar en cualquier momento en la Configuración del perfil, de acuerdo con las leyes de protección de datos aplicables.