PR

BIMobject adds 3D-printing and VR formats to its content creation solution

Louise Otto - 2017-09-14


BIMobject AB (“BIMobject”) today announces that the 3D-printing format STL and the Virtual Reality-format FBX have been made available for BIMscript® & LENA, a solution for creating digital building products. As of now, products created in BIMscript® & LENA will automatically be available in these file formats, adding value and possibilities for manufacturers, developers, and designers.



The BIMobject® content creation solution BIMscript® & LENA is enhanced with two additional output file formats: the STL format optimised for 3D-printing, and the Virtual Reality format FBX. The two new file formats are generated automatically in the content development process, creating direct links to be used for 3D-printing and Virtual as well as Augmented Reality solutions. Existing content can be updated to include the formats.

The stereolithographic STL format is the basis for all 3D-printers and is integrated into BIMscript® & LENA as an additional file format. This means that scale models and prototypes of parametric BIM objects can be printed more easily from a single source, without any file conversion. This will in turn improve the workflow for designers, who use 3D-printers to create physical models for presentations to building owners and building developers.

“Our unique development solution has taken a huge step forward: The new file formats add value to the process without meaning extra work for content developers. For manufacturers, offering a downloadable scale model of the building or interior product for 3D-printing is a great way to support designers and engineers in their work”, says Ben O’Donnell, Chief Technology Officer at BIMobject.

FBX is an adaptable file format that was originally developed for 3D-animation software. Integrated into BIMscript® & LENA, it allows users to access the created BIM objects directly from within a VR application such as BIMobject® VR and BIMobject® AR. The format thus offers manufacturers easier integration of their products into any VR solution, saving time and money, as well as maintaining an unbroken flow for all content creation. The content is made available to more designers for more types of possible use in the design, visualisation, user engagement, and sales processes.

“We already know that VR and AR are the next big thing, but the technology needs reliable product information and geometry. FBX turns it into a standard part of the process that can then easily be explored by solutions for real-time visualisation, online configurators, and walk-throughs in 3D. I think we’ll see a surge in the number of BIMscript developers and manufacturers using the technology”, says Ben O’Donnell.

BIMscript® & LENA consists of the scripting language BIMscript® and the plugin LENA, which let 3rd-party content developers and manufacturers create their own digital building products by importing native mechanical CAD geometry and optimising it for BIM objects. Developers can generate parametric, native BIM objects in a number of popular formats for industry-leading BIM applications. These BIM objects are then hosted on the platform BIMobject® Cloud, which serves as a Single Source of Truth for its over 500,000 professional registered users and more than 1,000 represented brands.

Originally published on September 13th, 2017.


News

"BIM is a communication, visualisation and prescription tool"

Elise Monot - 2018-12-07

News

“More and more design offices are working in BIM”

Elise Monot - 2018-11-28

News

Adapting to the needs of a global market

Nina Quist - 2018-11-09

PR

More content in the ever-growing BIMobject Cloud!

Carol Ping - 2018-11-09

News

“It’s the modern and smart way for us to manage our digital content”

Nina Quist - 2018-10-31

News

Tonda Pizza - Going global with BIM

Nina Quist - 2018-10-26

News

Building a brand with BIM

Nina Quist - 2018-10-26

BIMobject R&D Department presents: Augmented Reality

Johan Dyrssen - 2018-10-25

Introduction to BIMobject VR and AR

Ben ODonnell - 2018-10-25

BIMscript

Video: What is BIMscript?

Emil Augustsson - 2018-10-24

Digital Building

What is BIMobject Hercules?

Colin Ingram - 2018-10-19

News

"The demand is real and it's growing"

Nina Quist - 2018-10-18