Markenheldfoto

Saxonian bank in Leipzig, Germany

The Saxon bank "Sächsische Aufbaubank" of the Free State of Saxony provides fundings for companies, research institutes, as well as housing construction and urban development enerprises. A publicly accessible forest of concrete columns is located in front of the transparently designed building. The access from the underground car park to the staircase in the basement proves that sliding doors play a decisive role in the entrance experience. Function and design perfectly complement each other in the bi-parting version with glazed side door panels and glazed overhead panel. The low-profile sliding door has been executed in an elegant golden shade and serves as a porch system to prevent unpleasant draughts. It is equipped with a low-noise, long-life and automatic door locking system with mechanical manual unlocking on the inside. The door position and locking are monitored by the system. The installation was carried out on exposed concrete, which required extremely precise and neat work.