• Aignep Spa
Brand logo

Aignep Spa

Aignep started in 1976 in Bione (Brescia) as a contractor, producing fittings for the heating field, taking advantages from an industrial district specialized in the “taps and fittings” field. Nowadays the company produces a complete range of products, with its own brand in the FuidPower industry.

Quality and innovation are the motto of Aignep: the entire production is realized in Italy and it’s distributed worldwide. The only exception are some products dedicated to the North American market, which have to undertake local regulations, there they are perfected in the USA branch.

Aignep is part of the Bugatti Group (since 1923), which is made up of 4 companies of other fields: household products (Casa Bugatti), lighting (Landa), machine tools (Picchi) and FluidPower (Aignep).

Aignep exports in more than 100 countries thanks to an intensive distribution network and thanks to 10 branches located in USA, Spain, Switzerland, Brazil, France, Colombia, China, Russia, Germany and Singapore.

The distribution network and the branch companies allow Aignep to be always available for clients and to forward information to the Technical Dept. This Information in some case became new Aignep products, placed on the market.

The international dimension of Aignep it is also shown by the website and by all the technical documentation of every products, translated in 6 different languages.

Aignep has 5 division of products: fittings, quick couplings, automations, fluid control (Fluidity), air pipeline (Infinity).

Beside the standard production, Aignep designs and manufactures also customized solutions, providing assistance since the designing, with a real partnerships approach.

Products and solutions by Aignep reacts to different practical necessity: compressed air, automation, fluids distribution and even more complex processes which include stainless steel and special brass alloys.

The heart of Aignep products reside in the continuous innovation and in the technology expertise of Aignep’s human resources. Moreover Aignep it’s located in one of the most developed area of its field.

In the headquarter a Technical department is dedicated exclusively to the research and development of new products. This is combined with a control and testing department for prototype and solutions developed together with clients.

All the patents registered for product, processing and mounting are a clear demonstration of spirit of innovation.

Thanks to the automatic stock of Bione, Aignep can provide its products worldwide in short time.

With the Mobile App Aignep Scan it is possible to optimize the stock and forward the orders with a simple scan of the QR codes or Barcodes, that can be found directly on the product packaging or from labels that can be found on Aignep website.

Aignep provides set of catalogues and documents containing every kind of technical information. This together with an intensive distribution network, let clients to reach detailed information on every specific necessity.

  • Website
  • www.aignep.com/
  • Address
  • Via Don G. Bazzoli, 34, 25070 , Bione BS, Italy Italy
  • Phone
  • +39 0365 896626
Latest products
See all 92 productsBIMobject home
Image for PLUG-IN AIGNEP
Aignep Spa PLUG-IN AIGNEP
Image for Solenoid 30-36 Mm - Solenoids
Aignep Spa Solenoid 30-36 Mm - Solenoids
Image for 135° Connector 90140
Aignep Spa 135° Connector 90140
Image for 2 Ways Inclined Manifold Female - 90662
Aignep Spa 2 Ways Inclined Manifold Female - 90662
Image for 2 Ways Inclined Manifold Female Nptf - 90663
Aignep Spa 2 Ways Inclined Manifold Female Nptf - 90663
Image for 2 Ways Inclined Manifold Tube-Female - 90660
Aignep Spa 2 Ways Inclined Manifold Tube-Female - 90660
Image for 2 Ways Inclined Manifold Tube-Female - Inox316L - 90660X
Aignep Spa 2 Ways Inclined Manifold Tube-Female - Inox316L - 90660X
Image for 2 Ways Inclined Manifold Tube-Female Nptf - 90661
Aignep Spa 2 Ways Inclined Manifold Tube-Female Nptf - 90661
Image for 2 Ways Inclined Manifold Valve-Female - 90664
Aignep Spa 2 Ways Inclined Manifold Valve-Female - 90664
Image for 2 Ways Inclined Minifold Valve-Female Nptf - 90665
Aignep Spa 2 Ways Inclined Minifold Valve-Female Nptf - 90665
Image for 2 Ways Manifold - 90602
Aignep Spa 2 Ways Manifold - 90602
Image for 2 Ways Manifold - 90642
Aignep Spa 2 Ways Manifold - 90642