• Mapei
Brand logo

Mapei

Founded in 1937 in Milan, Mapei is today one of the most important producers of adhesives and complementary products for laying all types of floor and wall and coating materials, and is also specialised in other chemical products used in the building industry, such as waterproofing products, special mortars, admixtures for concrete, products for underground constructions and for the restoration of concrete and historical buildings. Mapei has built its strategy following three main guidelines: specialisation in the world of building by offering certified products and systems to meet the requirements of clients and market demand; internationalisation to be more in tune with local needs and to reduce transport costs to a minimum; Research and Development, which receives the most support from the Company in terms of both investments and human resources.

  • Website
  • www.mapei.com/
  • Address
  • Via Cafiero, 22, 20158, Milano Italy
  • Phone
  • +39 02 376731

Latest products

View all 34 products in searchBIMobject home
Image for RIPRISTINO MEDIANTE POSA DI PAVIMENTAZIONI RESILIENTI IN SOVRAPPOSIZIONE A VECCHIA CERAMICA ESISTENTE
Mapei RIPRISTINO MEDIANTE POSA DI PAVIMENTAZIONI RESILIENTI IN SOVRAPPOSIZIONE A VECCHIA CERAMICA ESISTENTE
Image for SISTEMA PER LA POSA DI LVT IN BAGNI E AMBIENTI UMIDI
Mapei SISTEMA PER LA POSA DI LVT IN BAGNI E AMBIENTI UMIDI
Image for SISTEMA PER LA POSA DI PAVIMENTAZIONI RESILIENTI
Mapei SISTEMA PER LA POSA DI PAVIMENTAZIONI RESILIENTI
Image for SISTEMA PER LA POSA DI PAVIMENTAZIONI RESILIENTI CONDUTTIVE O STATICO-DISSIPATIVE
Mapei SISTEMA PER LA POSA DI PAVIMENTAZIONI RESILIENTI CONDUTTIVE O STATICO-DISSIPATIVE
Image for Laying of porphyric cubes for elastic and draining driveway flooring according to uni 11714-1:2018 norm
Mapei Laying of porphyric cubes for elastic and draining driveway flooring according to uni 11714-1:2018 norm
Image for Breathable render for newly built masonry for healthy and comfortable surroundings (external with lime and cement-based products)
Mapei Breathable render for newly built masonry for healthy and comfortable surroundings (external with lime and cement-based products)