Buzzi & Buzzi was founded in 1990 by Pietro Buzzi and Marialuisa Chiari, two successful professionals who decided to cultivate and explain the insights and knowledge they had gained from years of experience in the lighting sector.
Since the early years, the company has relied on the contribution of renowned architects, thus recognizing the importance of design differentiation.
Technology and design come together to create new concepts of light: the result is objects which are genuinely different, not only from an aesthetic point of view, but also functional and technical.
Buzzi & Buzzi has established itself both nationally and internationally. Due to its alertness towards requests and modern trends, the company has specialized in proposing total recessed lighting products, while making the most of the Coral®'s technical performance.
The company has distinguished itself over the years through an ethical commitment based on its respect for the environment. This is reflected not only in the use of Coral®, which goes beyond the concept of zero impact and also plays an active role in improving the environment in the space where it is installed, but also through the choice of light sources which are mainly energy-saving and LED lightbulbs used extensively in Buzzi & Buzzi products.
Vos données personnelles peuvent être partagées avec des fabricants tiers en fonction de votre activité sur la plateforme. Vous pouvez vous y opposer à tout moment dans les paramètres de votre profil, conformément à la législation applicable en matière de protection des données