Publicar produtos
Imagem do heroi da marca

3-5 Squash Courts

When designing a mid-size squash centre of the size of 3 to 5 courts it is important to work very effectively with the space available. Placement of the courts is usually side by side or opposite to each other, possible is also a customized layout with a centre court and surrounding courts.The courts can also share side walls or front walls. Some courts can be dedicated to multifunctionality using the ASB Movable SideWall. Utilizing the surrounding walls of the building is very useful using ASB System40, or the self-standing ASB System100 walls can be used. The ideal solution in most of the cases is the combination of System40 and System100.