Petersen, a Carlisle company, manufactures PAC-CLAD metal cladding products in multiple gauges of steel and aluminum. PAC-CLAD architectural products include wall panel systems, standing-seam roof panel systems, soffit systems, perforated metal, fascia and coping systems, composite panels, column covers, coil and flat sheet. All are available in full 70% PVDF finish in many standard colors that include a 35-year finish warranty. Most colors meet LEED and Energy Star requirements, and are rated by the Cool Roof Rating Council. Founded in 1965. For information on the complete line of Petersen metal products call 800-PAC-CLAD, visit pac-clad.com or write to info@pac-clad.com.
Os seus dados pessoais poderão ser partilhados com fabricantes terceiros com base na sua atividade na plataforma. Pode cancelar a qualquer momento nas Definições de Perfil, em conformidade com as leis de proteção de dados aplicáveis.
Metal roof, wall panels help connect new mixed-use complex to its industrial past
The Raleigh Iron Works project, located in North Carolina’s high-tech Research Triangle, successfully revitalized a former iron foundry district into a thriving mixed-use hub. Opened in 2023, the development’s design pays homage to its industrial past, making extensive use of architectural metal roof and wall panels.
The centerpiece of the development is a pair of historic foundry structures—the Bow Truss and Double Gable buildings—which were originally part of a Peden Steel facility. After being abandoned in the early 2010s, developers Grubb & Ellis partnered with designers from LS3P and S9 to transform the derelict site into a vibrant space with a mix of retail, restaurants, and offices, along with a new multi-family structure.
Metal plays a prominent role in the design, reflecting the site’s history as an iron and steel producer. Both buildings feature standing-seam metal roofs, and the Bowtruss Building also features PAC-CLAD architectural metal wall cladding from Petersen. Installers used 40,000 sq. ft. of Petersen’s Tite-Loc Plus roofing panels and 30,000 sq. ft. of M-36 Corrugated wall panels for the project.
Petersen, a Carlisle company, manufactures PAC-CLAD architectural metal cladding systems in multiple gauges of steel and aluminum. PAC-CLAD products include wall panel systems, standing seam roof panel systems, flush- and reveal-joint wall panels, vented or solid soffit panels, perforated metal, coil and flat sheet, composite panels, and column covers, among others. All are available with a Kynar-based 70% PVDF Fluropon coating in 46 standard colors, which includes a 35-year finish warranty. Most of these colors meet LEED requirements and are rated by the Cool Roof Rating Council, with custom colors and weathertightness warranties also available.